ETrigTo (FB)

FUNCTION_BLOCK ETrigTo EXTENDS EdgeTriggeredTimingControlledBehaviourModelBase IMPLEMENTS IETrigTo

Base implementation of the PLCopen Edge Triggered Behavior Model (see: |IETrigTo|). For use, this block should be extended and the specific inputs and outputs must be supplemented. The output ``eErrorID` of the application-specific enum type ERROR must be added.

InOut:

Scope

Name

Type

Comment

Input

xExecute

BOOL

Rising edge: Starts defined operation

FALSE: Resets the defined operation after ready condition was reached

udiTimeOut

UDINT

Max. operating time for executing [µs], 0: No operating time limit

Output

xDone

BOOL

Ready condition reached

xBusy

BOOL

Operation is running

xError

BOOL

Error condition reached