INTERFACE ILevelControlled EXTENDS __SYSTEM.IQueryInterface
Used for IActionProvider instances whose behaviour model requires a xEnable input
See Level Controlled Function Blocks for more information about the meaning of the xEnable input.
This decorator is referenced by the following interfaces: ILCon (ITF) | ILConTl (ITF) | ILConTlTo (ITF) | ILConTo (ITF) | ILConC (ITF) | ILConTlC (ITF)