IoDrvEtherNetIPAdapter.SetAttributeValue (METH)

METHOD SetAttributeValue : UDINT

This method is called, if an default attribute of an EtherNet/IP Adapter needs to be changed. Only specific attributes can be changed.

InOut:

Scope

Name

Type

Return

SetAttributeValue

UDINT

Input

uiClass

UINT

dwInstance

DWORD

wAttribute

WORD

pData

POINTER TO BYTE

Output

xDone

BOOL

xError

BOOL