DTCBufferWriter (FB)

FUNCTION_BLOCK DTCBufferWriter EXTENDS DTCHandlerBase

This function block can be connected to a DM1_Read or DM2_Read function block. As long as xEnable is TRUE it receives DTCs and writes it to a memory buffer provided by pDTCBuffer. If a complete diagnostic message was received output xReceived becomes TRUE for one cycle and pDTCBuffer contains received DTCs. If buffer is too small DTCs can be lost (see output udiDTCLostCount).

Note

Output values and Data in pDTCBuffer is only valid as long as xReceived is TRUE (for one cycle).

InOut:

Scope

Name

Type

Comment

Inherited from

Input

xEnable

BOOL

TRUE: Action starts

FALSE: Action stops, outputs xDone, xBusy, xError are resetted

LTrig

Output

xDone

BOOL

TRUE: Action successfully completed

LTrig

xBusy

BOOL

TRUE: Function block active

LTrig

xError

BOOL

TRUE: Error occurred, function block aborts action

FALSE: No error

LTrig

Input

itfDTCHandlerList

IDTCHandlerList

DMx_Read instance

DTCHandlerBase

Output

eError

ERROR

detailed error information if xError is TRUE

DTCHandlerBase

Input

pDTCBuffer

POINTER TO DTC

Pointer to ARRAY OF DTC. If xReceived is TRUE buffer contains received DTC information. Note: Data is only valid as long as xReceived is TRUE.

udiDTCBufferCount

UDINT

Number of DTCs fitting into pDTCBuffer

Output

udiDTCReceiveCount

UDINT

Number of DTCs written to pDTCBuffer. Only valid if xReceived is TRUE.

udiDTCLostCount

UDINT

Number of dismissed DTCs. If greater 0 buffer is too small.

xReceived

BOOL

TRUE for one cycle if a diagnostic message was received. pDTCBuffer contains DTC information.