ControllerConfigUtil.UpdateStationName (METH)

METHOD UpdateStationName : ConfigError

Change the configured station name of the slave configuration.

Only possible if the connection to the slave is not active.

InOut:

Scope

Name

Type

Comment

Return

UpdateStationName

ConfigError

Input

pnDevice

DED.IDevice

A Profinet Controllers's Slave-Config node

StationName

STRING(240)

Stationname