ChannelProperties (STRUCT)

TYPE ChannelProperties : STRUCT

Information on a specific channel

InOut:

Name

Type

Initial

Comment

ChannelType

ChannelProperties_Type

ChannelProperties_Type.Unspecified

size / datatype of a channel (so far a matchingtype exists).

Accumulative

BOOL

FALSE

TRUE : the source is a channel group.

FALSE : the source is a specific channel or the whole submodule

Direction

DiagnosisDirection

DiagnosisDirection.Undefined

The direction of the affected IO-data