DCP_SetOptions (STRUCT)

TYPE DCP_SetOptions : STRUCT

DCP-Options that can be written to a Profinet device, see DCP_Set.

InOut:

Name

Type

Comment

StationName

BIT

IPSettings

BIT

Signal

BIT

Flash a LED or an alternative signalization with duration of 3 s (frequency e.g. 1 Hz (500ms on, 500 ms off).