ID
|
DWORD
|
unique (within project) ID of device. Use with CommFB function blocks.
|
StationName
|
STRING(240)
|
stationname of the Profinet device
|
VendorID
|
UINT
|
vendor ident. number
|
DeviceID
|
UINT
|
device / product ident. number
|
Instance
|
UINT
|
instance number
|
IPSettings
|
IPParameterValue
|
currently configured IP-address, subnetmask, gateway.
|
xEnabled
|
BOOL
|
device enabled
|
xRunning
|
BOOL
|
Slave is in cyclic data exchange.
|
xError
|
BOOL
|
Communication error. PNIOStatus displays reason.
|
PNIOStatus
|
UDINT
|
The current PNIO Status of the device.
|
xDiagnosis
|
BOOL
|
Any module of the slave has a diagnosis entry.
|
xModuleDiff
|
BOOL
|
The module configuration is not matching (wrong or missing).
|