DiagnosisInformationUSI (STRUCT)

TYPE DiagnosisInformationUSI : STRUCT

Diagnosis information in USI format

InOut:

Name

Type

Initial

Comment

Severity

DiagnosisSeverity

DiagnosisSeverity.Undefined

Severity of the diagnosis entry

USI

UINT

UserStructureIdentifier - expresses the type of diagnosis

DataLength

UINT

The length of the diagnosis data that is provided in field ManufacturerData

ManufacturerData

ARRAY [0..(Constants.MAX_SUBMODULE_ManufacturerDataLen - 1)] OF BYTE

Manufacturer specific diagnosis data