IProjectSettingsExtension

class

IProjectSettingsExtension.

IProjectSettingsExtension

Bases: object

This interface allows the modification of the project settings.

multicarrier_configuration

Contains Multicarrier related project settings.

Note

The MultiCarrier Addon must be installed to use this property.

Returns

The IMulticarrierConfiguration instance or None.