Output for signaling "Function block activated/not activated".
Data type: BOOL
Connection: If required, the signal can be connected to a standard variable of the BOOL data type or to other standard functions/function blocks.
|
Value |
Description |
|---|---|
|
TRUE |
Function block is activated (Activate = TRUE) and the output parameters represent the present state of the safety-related function. |
|
FALSE |
Function block is not activated (Activate = FALSE) and all outputs of the function block are switched to FALSE/SAFEFALSE. |