SMC_GSentenceJumpBuffer (FB)

FUNCTION_BLOCK SMC_GSentenceJumpBuffer

This function block buffers g-code sentences in order to avoid a full restart of the g-code file on jumps (G20). It must be used before the SMC_NCNavigator function block. Note: this function block is part of SMC_ReadNCFile2, so it is not necessary to instantiate it by hand.

InOut:

Scope

Name

Type

Comment

Inout

sentencesOut

SMC_GSentenceQueue

The output sentence queue

sentencesIn

SMC_GSentenceQueue

The input sentence queue

Input

bExecute

BOOL

While TRUE, the function block is active.

Output

bBusy

BOOL

TRUE while execution of function block is not finished.

bError

BOOL

TRUE signals that an error has occurred within the function block.

ErrorID

SMC_ERROR

Error identification, SMC_ERROR

errorPos

SMC_NC_SourcePosition

The source-position where an error has been detected.

numHits

UDINT

The number of jump targets found in the buffer. Reset at rising edge of bExecute.

numMisses

UDINT

The number of jump targets not found in the buffer. Reset at rising edge of bExecute.