FUNCTION_BLOCK SMC_NC_PrependDefaults
This function block is used internally by SMC_ReadNCFile2 to prepend a sentence containing the given defaults, e.g. 'N0 G17 F25 E1000 E-2000'. If SMC_ReadNCFile2 is used, there is not need to use this function block.
Important: this function block will prepend the defaults again after a jump command in the out queue. So it should be used before any buffering function blocks such the jump buffer. It should be called before SMC_NCNavigator as well, because the navigator will handle the jumps to unknown jump targets.
InOut:
|
Scope
|
Name
|
Type
|
Comment
|
Inout
|
sentencesOut
|
SMC_GSentenceQueue
|
The output sentence queue
|
sentencesIn
|
SMC_GSentenceQueue
|
The input sentence queue
|
Input
|
bExecute
|
BOOL
|
|
fDefaultVel
|
LREAL
|
Default velocity; used if the velocity (F-word) is not specified inside the CNC file.
|
fDefaultAccel
|
LREAL
|
Default acceleration; used if acceleration (E+ word) is not specified inside the CNC file
|
fDefaultDecel
|
LREAL
|
Default deceleration (E- word); used if deceleration is not specified inside the CNC file
|
fDefaultVelFF
|
LREAL
|
Default velocity for fast forward (G0), FF word. It is used if no velocity is specified inside the CNC file.
|
fDefaultAccelFF
|
LREAL
|
Default acceleration for fast forward (G0), EF+ word. It is used if no acceleration is specified inside the CNC file.
|
fDefaultDecelFF
|
LREAL
|
Default deceleration for fast forward (G0), EF- word. A non-negative value is expected. It is used if no deceleration is specified inside the CNC file.
|
b3DMode
|
BOOL
|
If TRUE, a G17 command (activation of 3D-mode) is executed implicitly.
|
Output
|
bBusy
|
BOOL
|
|
bError
|
BOOL
|
|
ErrorID
|
SMC_ERROR
|
|
errorPos
|
SMC_NC_SourcePosition
|
|
|