FUNCTION SMC_RecalculateHelpMarks : BOOL
This function recalculates the positions of the helpmarks if the length of one object has changed from l, starting at the beginning iDir = 1 or end iDir = -1.
Scope
Name
Type
Return
SMC_RecalculateHelpMarks
BOOL
Input
pg
POINTER TO SMC_GeoInfo
l
LREAL
iDir
INT