SMC_SEGMENT (STRUCT)

TYPE SMC_SEGMENT : STRUCT

This structure is used internally by the SMC_Interpolator . It represents a path segment of fixed length in which a certain acceleration shape is used.

InOut:

Name

Type

Comment

eType

SMC_SEGMENTTYPE

ACC, CONST, DEC, M

dLength

LREAL

Object length

dTime

LREAL

Needed time for interpolation

dVelStart

LREAL

Velocity at the beginning of the segment

dVelEnd

LREAL

Velocity at the end of the segment

iStartObj

INT

Position of the start object in the queue

dPosInStartObj

LREAL

Beginning of segment relative to the start point of the start object

iDestObj

INT

Position of the last object in the queue

dPosInDestObj

LREAL

End of segment relative to the start point of the destination object

dAccStart

LREAL

Start acceleration (signed)

dAccEnd

LREAL

End acceleration (signed)

dJerk

LREAL

Jerk (signed), only used for changing acceleration