SMC_UnitVectorToRPY (FB)

FUNCTION_BLOCK SMC_UnitVectorToRPY

This function block will calculate the RPY-angle (referring to the old coordinate system) from the unit vectors of the new coordinate system.

For detailed information of transformation modules see the survey on Coordinate Transformations.

InOut:

Scope

Name

Type

Comment

Input

vX

SMC_Vector3d

x-coordinate of unit vector of new coordinate system (in respect of old coordinate system)

vY

SMC_Vector3d

y-coordinate of unit vector of new coordinate system (in respect of old coordinate system)

vZ

SMC_Vector3d

z-coordinate of unit vector of new coordinate system (in respect of old coordinate system)

Output

dA

LREAL

Roll angle in radian measure

dB

LREAL

Pitch angle in radian measure

dC

LREAL

Yaw angle in radian measure

bError

BOOL

Signals, that an error has occurred within the function block

nError

WORD

Error description:

  • 1: No error (bError = FALSE)

  • 2: Vectors do not have length 1

  • 3: Vectors are not orthogonal

  • 4: No right hand system