System
SysFile
3.5.15.0
System|SysLibs
3S - Smart Software Solutions GmbH
This library provides access to the file functionality of the runtime system.
ACCESS_MODE (ENUM)
SYS_FILETIME (STRUCT)
SYS_FILE_STATUS (ENUM)
SysFileClose (FUN)
SysFileCopy (FUN)
SysFileDelete (FUN)
SysFileDeleteByHandle (FUN)
SysFileEOF (FUN)
SysFileFlush (FUN)
SysFileGetName (FUN)
SysFileGetName2 (FUN)
SysFileGetPath (FUN)
SysFileGetPos (FUN)
SysFileGetSize (FUN)
SysFileGetSizeByHandle (FUN)
SysFileGetStatus (FUN)
SysFileGetStatus2 (FUN)
SysFileGetTime (FUN)
SysFileOpen (FUN)
SysFileRead (FUN)
SysFileRename (FUN)
SysFileSetPos (FUN)
SysFileTruncate (FUN)
SysFileWrite (FUN)
[1]
Based on SysFile.library, last modified 24.07.2019, 09:08:13. LibDoc 3.5.16.0
The content file SysFile.clean.json was generated with CODESYS V3.5 SP15 on 24.07.2019, 09:08:15.