Symbol:
Function: This tab allows for the configuration and the transfer of controller certificates for encrypted communication with the controller.
Call: Menu bar: View.
Requirement: The CODESYS Security Agent add-on product is installed.
For more information about this topic, refer to the CODESYS Help:
The Devices tab shows all PLC devices configured in the project and their certificate store. If the communication path to the controller is configured, then you see the certificates that are stored in memory. Here you can create and configure new certificates on the controller.
Left side: Information |
Devices and certificate store
Shows the individual devices For example, there are the following categories for CODESYS Control Win V3:
|
Toolbar (left side) |
|
Right side: |
If the active path to the controller is set and a device node is selected, then every use case for controller certificates is displayed on the right side.
As long as a certificate is not available for one of these use cases, it is displayed with the When a certificate store is selected on the left side, all certificates in it are displayed on the right side with the following information: Information: Use case (currently the controller component in question is displayed: for example CmpSecureChannel.) Created for: Name of the computer for which the certificate was created (for example, MyLocalPC) Created by: Name of the computer on which the certificate was created (for example, MyLocalPC) Valid as of: Date (for example, 07/20/2017 15:09:29) Valid until: Date (for example, 07/20/2022 00:00:00) Thumbprint: Hash value from specific properties of the certificate for purposes of identification (for example, 279e1a46b86bd636c8e6f19fd51c222469ec49a8) Double-clicking a certificate entry opens the default Windows Certificate dialog. Here you can import a controller certificate in the Windows Certificate Store to the directory Controller certificates so that it is available for encryption of download, online change, and boot application. If multiple certificates are available for one use case, then the system follows the steps below to determine the certificate that is used:
|
Drag&Drop: Moving of the certificate to another certificate store of the same device Double-clicking a certificate entry opens the default Windows dialog for displaying all certificate information. |
|
Toolbar (right side) |
The Certificate Settings dialog opens for configuring the Validity period of the certificate and the Key length for the private key. Clicking OK saves the specified values in the CODESYS options. The values are reset at the next operation. As long as the certificate is being created, "(computing)" is shown after the use case. You cannot cancel the creation operation, but you can close and continue working with the Security Screen.
|