Command 'Set variables'

Function: This command opens the Offline values of variables dialog box. The variables of the CNC program can be defined here for offline mode.

Call: Menu bar: CNC .

Requirement: A CNC path is open in the editor.

Dialog box 'Offline values of variables'

Variable

Variable of the CNC program

Example: G_X

If the variable is shown in gray italics, then it is not being used in the CNC program.

Value

Configured offline value

Example: 100

Set to online values

The values are overwritten with the values that are currently assigned in the application.

Requirement: The command is available it the application is running and the CNC editor is in online mode. Then it is possible to load the online values.

OK

If the values are valid, then they are applied in the CNC program and the path of the editor is refreshed.

See also