Symbol:
Function: The command commits changes that were made in CODESYS to the SVN repository. The Commit dialog opens for this purpose.
Call:
Context menu: to commit exactly this object
to commit all changes in the project at the same time
Requirement: At least one object was modified. An object whose contents have been modified is overlaid in the object tree with the
,
, or
symbol.
When you execute the command, the lock on the objects to be committed is lifted automatically.
See also
|
URL in SVN repository
Example: |
|
|
Log message |
Type in a log message that comments your change.
Example: |
|
Recent Messages |
Opens the Recent Messages dialog for displaying the last log messages. You can click a log message to accept it. |
|
|
List of objects that were changed and can therefore be committed. The SVN URLs mirror the hierarchy of the object in the SVN repository. The objects are highlighted in color according to the object status:
The list also contains objects which have not been modified but have a lock. This helps to prevent locking from going unnoticed in the repository. Double-click an object in order to open the compare dialog. The revision of the working copy is compared with the base revision. The compare dialog also opens when you click Compare in the context menu. Right-click an object in order to open the context menu. Note: When the Commit Project command has been executed, a list of objects is shown here. When the Commit command is applied to a specific object, only this object is shown (if modified or locked) and its modified or locked child objects. |
|
Object |
Example: |
|
Text status |
Object status in CODESYS
|
|
Property status |
Status of the metadata of the object
|
|
Lock |
If the object has a lock, then it is shown here the user who applied the lock.
Example: |
|
Description |
Display of the log message |
|
Select/Deselect All |
|
|
Keep Locks |
|
|
Keep Change Lists: |
|
|
Update After Commit (recommended) |
|
|
Button Update Project |
Updates the project Hint: Prevent conflicts by committing a previously updated project/object. |
|
OK Keyboard shortcut Ctrl+Enter Keyboard shortcut Ctrl+Enter |
Checks the working copy first. Starts the commit of changes when the working copy is current. Opens a dialog when the working copy is outdated. You can then select from the following:
Note: The history of the commit is displayed in the Messages view. The messages are highlighted in color.
|
Handling external objects If the external object is in the same SVN repository, then changes in this external object are listed in the commit dialog and committed together with the internal project. If an external object is in another SVN repository, then you are notified about changes in the external project and you have to commit these separately.
An external object has the externals property.
See also