Symbol:
Function: This command opens the Revert dialog. In the dialog, select the objects whose local changes should be reverted, and those that are reverted to the state of the base revision of the working copy.
Call:
Menu bar:
.
If you select nothing or the main node in the device tree, then all modified objects are listed in this dialog (Revert project). If you selected one or more objects, then only the changes to this object are listed and recursively their sub-objects (Revert).
Group externals |
|
Keep locks |
|
Select/deselect all |
When external objects are deleted, CODESYS SVN cannot restore this data in SVN offline mode. The user is prompted how to proceed:
Switch back to SVN online mode and call the external objects.
Connect now to the SVN server one time in order to complete the current operation, but afterwards switch back to SVN offline mode.
Skip the retrieval of the external objects. They can be fetched later by updating the project.
See also