Command 'Switch'

Symbol:

Function: This command opens the SVN switch dialog. In this dialog, you specify a URL in the SVN repository to which the current working copy of the project is updated. The command switches a project from a branch or tag to another.

Call: Menu bar: Project ‣ SVN .

Requirement: The project is versioned.

Dialog 'SVN switch'

From

Current SVN URL of the project

To

Input field for the target URL in SVN

  • HEAD: The Select revision dialog opens.

  • : The SVN Repository Browser dialog opens. There you select the target URL in the SVN repository.

See also