Function: This command removes an unversioned object from the ignore list so that the object is checked by default on commit.
Call: Context menu: SVN
Requirement: The command Ignore on commit was executed for the object. The object is marked with the
symbol.
See also