Dialog 'Project Settings' - 'SVN Settings'

Symbol:

Function: The behavior of the integrated SVN version control system is configured in this dialog.

Call: Menu bar: Project ‣ Project Settings (SVN Settings).

Requirement: A project is open.

Automatic locking and merging

With these settings, you can overwrite the default settings that were made in the dialog Tools ‣ Options , category SVN Settings.

Merge

Behavior for the commands Update, Merge, or Switch, when both sides (working copy and SVN repository) have changed from the base version.

Locks

Behavior such as CODESYS SVN objects when they are changed locally.

Marker

Behavior for conflicts

Settings SVN version info

Create SVN_VERSION_INFO constants for IEC access

: The object SVN_VERSION_INFO is created and includes global constants or variables for the project metadata.

: The object SVN_VERSION_INFO is not available.

When you activate the option, the object is created automatically. When you deactivate the option, the object is removed from the project automatically.

See also