Object: EtherNet/IP Target
The upper area of this tab displays a list of all configured connections. When a connection is selected, the associated assemblies in the lower area of the tab are displayed.
Add |
Opens the dialog box Select Parameters. |
Delete |
Deletes all selected parameters. |
Move up Move down |
Moves the selected parameter within the list. The order in the list determines the order in the I/O mapping. |
Name Bit Length Help String |
These values can be changed by double-clicking into the text field. |
Also see
Show parameter groups |
Individual parameters from this list can be selected and added to the list of assemblies by clicking OK. |
Generic parameter |
|