Tab 'EtherNet/IP Target - User-Defined Parameters'

Object: EtherNet/IP Target

This tab displays all additional parameters that are transmitted once only into the bus system during the phase of the starting procedure allotted to this.

Notice

The user parameters are also transmitted again when a connection is reestablished, for example after the failure of a remote adapter.

New

Opens the Select Parameters dialog for adding a new parameter. The new parameter is inserted before the selected line.

Edit

Opens the Select Parameters dialog for changing an existing parameter.

Move Up, Move Down

Changes the order of the user parameters. The order of the parameters in the list corresponds to the order at the initialization.

Value

The value of the respective parameter can be directly changed by double-clicking the value. If applicable, a list box opens containing possible values.

Abort on Error

: On occurrence of an error the complete transmission of the parameters is aborted.

Jump to Line on Error

: In the event of an error the program resumes with the line specified in the Next Line column. A complete block can thus be skipped during the initialisation or a return can be defined.

Please note: A return can cause an infinite loop when if it is never possible to write a specific parameter.

See also