PROFINET Controller - Media Redundancy

Object: PROFINET Controller

This tab is used to configure the media redundancy protocol (MRP) for the PROFINET devices addressed by this PROFINET controller.

<group name>

Enable

: Activates the MRP domain

MRP domain

Name of the MRP ring configuration

Device

Name of the device in the device tree or the name of the respective function block

Station name

The station name of the device

MRP instance

Index of the MRP ring (assigned automatically). Some devices support the participation in multiple MRP domains.

MRP role

Role of the device in the MRP ring

  • Off

  • Client

  • Manager

  • Manager_Auto

Ring Port 1

Ring Port 2

Ports of the ring that are part of the MRP ring. The neighboring port is displayed in brackets.

See also