Tab 'Modbus Slave Serial - General'

Object: Modbus Slave Serial

This tab includes the basic settings for communication via the serial port.

Modbus RTU/ASCII

Slave address [1..247]

Address of a serial Modbus device (value between 1 and 247)

Response timeout [ms]

Time interval for the master to wait for the response from the slave. This is especially configured for this slave node and overwrites the general response timeout setting of the respective master.

See also