Tab 'ModbusTCP Slave - General'

Object: Modbus SlaveTCP

This tab includes the basic settings for network communication.

Modbus TCP

Slave IP address

Response timeout

Time interval for the master to wait for the response from the slave. This is especially configured for this slave node and overwrites the general response timeout setting of the respective master.

Port

Port number (TCP/IP) of the slave 502 is default for Modbus

Note

The communication settings can be changed at runtime using the method UpdateCommunicationSettings. This method is available for the implicitly generated function block of this Modbus slave.

See also