Function Block 'IoDrvModbusTCPSlave'

Library:IoDrvModbusTCPSlave

This block is generated for each Modbus TCP slave device in the device tree.

Outputs (VAR_OUTPUT)

Name

Data type

Initial value

Description

xInternalError

Bool

FALSE

Unrecoverable internal error (for example, if mem-aloc or license is missing)

uiClientConnections

Bool

FALSE

Number of currently established client connections (TCP/IP)