Command 'Add Elements for Alarm Acknowledgement'

Symbol:

Function: This command adds buttons automatically to the visualization for acknowledging alarms. It opens an assistant for inserting controls below the table.

Call: Menu bar: Visualization ; context menu of visualization element "Alarm table"

Requirement: An "Alarm table" visualization element is selected.

Dialog box 'Alarm Table Wizard'

Type of element(s) to insert

  • Button

  • Rectangle

Action

: A button or a rectangle with the selected function is added to the visualization.

Variable

If you have already specified a variable for an action, then this is displayed here in the Variable column. If you have not defined a variable yet, then a local visualization variable is created automatically.

See also