Command 'Export Trace Configuration'

Function: This command opens the Export Trace Configuration dialog box.

Call: context menu (right-click) the upper node in the tree view of the trace configuration.

Requirement: The dialog box Trace Configuration is active and the name of the trace configuration is selected in the tree view (example: Visu_Trace1).

Dialog box 'Export Trace Configuration'

This dialog is used for saving the trace configuration to a text file that can be read by the runtime system.

File name

Name of text file to be created.

File type

Trace file (*.trace): Format that the runtime system component CmpTraceMgr expects for reading.

See also