Symbol:
Function: When you execute this command in or in the context menu, the Edit Display Settings dialog box opens.
Call:
Menu bar:
Context menu of a Trend element in the visualization editor
Property Display Settings
Requirement: A trend is selected in the active visualization editor.
|
|
|
|
|
Minimum |
Start value of the range Requirement: Fixed is activated. |
|
Maximum |
End value of the range Requirement: Fixed is activated. |
|
Grid |
|
|
Description |
|
|
Fixed spacing |
|
|
Distance |
Distance between tick marks (example: |
|
Subdivisions |
Number of subdivisions between tick marks (example: |
|
From visualization style |
Background color as defined in the visualization style |
|
Draw background |
Background color that is selected in the lower input field |
|
No background |
Trend diagram with transparent background |
|
Background color of the trend diagram |
Requirement: Draw background is activated. |
|
Add y-axis |
Extends the trend diagram by one y-axis Result: The Trend recording editor contains an extended selection of y-axes in the Additional axes option of the Variable Settings. |
|
Delete y-axis |
Deletes the y-axis of the visible tab. |
See also