Dialog 'Create HMI Project - Select Perspective'

Function: This dialog box is part of the wizard that opens when you create a new project with the HMI project template. This is used for selecting the perspective for the current project. The perspective can be modified later at any time by clicking Select Perspective.

Call: Automatically after the Create HMI Project - Add Objects dialog box

See also

HMI perspective

CODESYS perspective

: Perspective to open the new project.

Preview

Preview of the project organization in the new project according to the configuration in the wizard.

Abort

The configuration is applied, and a new HMI project is created and opened in CODESYS. Now the basic framework of an HMI project has been created.

See also