Function: The dialog displays the currently used visualization style of the project. The visualization style can be updated here.
Call: Main menu Visualization Styles
, tab
For the following visualization styles currently in use, newer versions are available: |
|
Visualization Styles |
Version of the currently set visualization style of the opened project. |
Current |
Current version of the visualization style, for example |
Recommended |
Recommenden version of the visualization style, for example |
Action |
|
Do not update |
The visualization style of the project remains unchanged. |
Update to x.x.x.x |
CODESYS updates the project to the version of the chosen visualization style. |
Check for updates when loading the project |
|
Set All to Newest |
CODESYS updates the version. |
See also