Function: The dialog box lists installed symbol libraries and enables you to assign a symbol library to the project.
Call: Main menu Visualization Symbols.
, tab
Requirement: The opened project contains a visualization and has been saved with a compiler version of < 3.5.7.0
. CODESYS knows symbol libraries from compiler version 3.5.7.0
.
Symbol libraries |
List of all installed symbol libraries |
Active |
|
See also