Symbol:
Function: This dialog box is for the configuration of the project-wide settings for objects of the type Visualization.
Call: Main menu Visualization
, categoryRequirement: A project is open.
Text list files |
Directory containing text lists that are available in the project for configuring texts for different languages. CODESYS uses the directory, for example, when exporting or importing text lists.
After clicking on |
Image files |
Directory containing image files that are available in the project. Multiple folders are separated with a semicolon. CODESYS uses the directory, for example, when exporting or importing image files.
After clicking on |
Activate property handling in all element properties |
Requirement: Your IEC code contains at least one object of the type Interface property, i.e. a property
|
See also
Symbol Libraries |
List of all installed symbol libraries, for example |
Active |
|
See also