Function: The recording rate of the Trace visualization element is configured in this dialog box.
Call
Properties: Trace , Advanced
Context menu: Advanced
,Requirement: A trace is selected in the active visualization editor.
Measurement in every nth cycle |
The task where the trace is running is the basis for the measurement. The measurement interval is a multiple of the trace task according to the selected value. The measurement interval is displayed on the right side. |
Buffer size (samples). |
The number of measurements is calculated according to the time range of the x-axis. |
See also