Function: The dialog requests you, after changing an interface in the visualization references concerned, to re-assign the variables for the parameter transfer.
Call: The dialog appears automatically.
Requirement: You have changed the interface of a visualization, for example by adding an additional variable. After that you have selected either the menu command or or opened a visualization.
|
Parameter |
Hierarchical structure of the interface parameters as a tree view |
|
|
Top node of the visualization hierarchy with the name of the visualization. This contains a Frame or a Tabs control. |
|
|
Name of the element ( typ Frame, or Tabs) |
|
|
Name of the referenced visualization |
|
|
Interface of the referenced visualization with the new parameters You can edit the parameter transfer here. |
|
|
Interface of the referenced visualization with the previously valid parameters You cannot edit the parameter transfer, but you can use it as a template. |
|
|
Variable for the parameter transfer ( |
|
|
Variable for the parameter transfer ( |
|
Type |
Data type of the variable
Example: |
|
Value |
Variable that is transferred as a parameter and with whose value the visualization is initialized during instantiation.
Example:
If the variable lies under the current interface, which is marked in the tree view with
|
|
Copy |
Link to copy an assignment from the Value column. Requirement: An assignment is selected. |
|
Paste |
Link to insert an assignment Requirement: You have copied an assignment. |
|
OK |
Click on the button to close the dialog and confirm the changes made under (Recent). Result: The assignment is entered in the References property and on the Interface Editor tab. |
See also