Visualization Editor

The visualization editor opens after a double-click on a visualization object.

    1. Graphical editor: this is where you create a visualization from the visualization elements that are provided in the view Tools.

    1. View Tools: available visualization elements

    1. View Properties: configuration editor for the visualization element currently selected in the editor area

    1. Menu Visualization: commands for working in the visualization editor

Amongst other things, the menu Visualization contains commands for opening additional editors:

    1. Interface Editor: declaration of variables via which the references of the visualization can be parameterized.

    1. Hotkeys Configuration: definition of shortcuts for inputs on the visualization in online mode.

    1. Elementlist: List of all elements used in the visualization, possibility to change their position on the z-axis.

See also