Methods of the Dialog Manager

Visualizations that have the visualization type Dialog and serve as input requests are automatically instanced and managed by the internal dialog manager.

The dialog manager can be accessed in the application via the similarly internal visualization manager by calling the method GetDialogManager.

The dialog manager has the following methods for handling a dialog.

Notice

You can program the method calls in function blocks or functions that are themselves called from the visualization or via the action Execute ST code.

In addition, you can program the method calls in the application code. Make sure that the call runs in the VISU_TASK. The behavior is undefined if this is not the case.

See also

Method 'GetDialog'

Supplies the instance (IVisualisationDialog) of the dialog whose name is transferred.

Inputs (VAR_INPUT)

Name

Data type

Description

stName

STRING

Name of the dialog

Outputs (VAR_OUTPUT)

Name

Data type

Description

GetDialog

VisuElems.IVisualisationDialog

Instance (IVisualisationDialog) of the dialog

Method 'GetClientInterface'

Supplies a pointer to the dialog structure.

Note

Dialog data are held for each display variant.

Inputs (VAR_INPUT)

Name

Data type

Description

dialog

VisuElems.IVisualisationDialog

Name of the visualization

pClient

POINTER TO VisuElems.IVisualisationDialogVisuStructClientData

Pointer to the display variants

Outputs (VAR_OUTPUT)

Name

Data type

Description

GetClientInterface

Example: POINTER TO Login_VISU_STRUCT

Pointer to the dialog structure.

Method 'OpenDialog'

Opens the dialog for the client.

Note

In addition there is the extended method 'OpenDialog(Number)' .

Inputs (VAR_INPUT)

Name

Data type

Description

dialog

VisuElems.IVisualisationDialog

Name of the visualization

pClient

POINTER TO VisuElems.VisuStructClientData

bModal

BOOL

pRect

POINTER TO

Outputs (VAR_OUTPUT)

Name

Data type

Description

OpenDialog

Method 'CloseDialog'

Closes the dialog for the client.

Inputs (VAR_INPUT)

Name

Data type

Description

dialog

VisuElems.IVisualisationDialog

Name of the visualization

pClient

POINTER TO VisuElems.VisuStructClientData

Outputs (VAR_OUTPUT)

Name

Data type

Description

CloseDialog