Symbol:
The User management tab is used for creating and configuring the user management for visualizations and their users and groups.
If a user management has not been configured yet, then the following buttons are available: |
|
Create Empty User Management |
The user management opens. The None group is created. |
Create User Management with Default Groups and Users |
The user management opens. The following groups and users are created:
|
Requirement: The project includes several devices with a visualization user management. |
|
Use local user management |
The user management of this visualization manager is used for the visualization. |
Use remote user management |
Drop-down list with all devices of the project that have their own visualization user management. |
Even if there are no display variants of the visualization in the application, it may be required that the visualization user management is located on the controller. This is the case, for example, when HMIs connect to the controller.
Requirement: The visualization does not have any display variants or only HMI Visualizations objects. This means that the objects Web Visualization, Target Visualization, or Remote Target Visualization are inserted below the visualization manager. |
|
Use user management in PLC: This option must be activated if HMIs should be connected to this central user management. |
|
Group Name |
When you click the node, all users are listed that belong to the group. |
Automatic Logout |
|
Logout Time |
Input field for integer value Drop-down list for time unit Min, Sec, or Hr |
Permission to Change User Data |
|
Description |
The text is visible in the development system only. It is not downloaded to the controller. |
ID |
Unique ID for each group. Assigned automatically by the system. |
Add a new group |
In the last row of the table, click in the Group Name field and specify the name for the new group. |
Delete a group |
Select a group and press Del. The None group cannot be deleted. |
Update Visualizations / Hotkeys |
Opens the Update Visualizations and Hotkeys dialog box. Update, if groups were changed at a time when visualizations or keyboard shortcuts already had restricted permissions. |
List Usage of Groups |
List of visualizations and keyboard shortcuts with restricted permissions. The list is displayed in the Messages view. |
Export Groups for Global Visualizations |
The defined group names are transmitted to Use the following user group list for the visualization. The list can be changed there as well. . They are then listed in |
Delete Complete User Management |
The user management is deleted and the start view is shown with the following buttons: Create Empty User Management and Create User Management with Default Groups and Users. |
Export User Management |
The drop-down list opens.
A standard dialog opens for saving the user management as a CSV file with any name in any directory. |
Import User Management |
A standard dialog opens for importing a user management. the user management must be a CSV file. |
|
Moves the selected group one line up/down, thus changing the hierarchy of the group. A group of a higher hierarchy cannot have fewer permissions for an element than a group of a lower hierarchy. |
This dialog updates only visualization elements and keyboard shortcuts with configured permissions. |
|
Add New Group |
Drop-down list with all new created groups of this user management. Requirement: A new user group was created. |
Setting for New Group |
|
Delete Not Existing Groups |
If no affected visualization elements or keyboard shortcuts are found for updating, then this is displayed as a message in the Messages view (Visualization category). |
Rename Groups |
|
Update |
Updates the permissions of the affected visualization elements and keyboard shortcuts |
Login name |
Name for the user to log in to the visualization at runtime. This name is unique. |
Full name |
This name may exist more than one time in the user management. |
Password |
Encrypted by CODESYS. By default, the Login name is displayed here. If you click the Password field of a selected line, then the Change password dialog box opens. |
User group |
Group(s) that the user belongs to. Clicking the User group field of a selected user opens the dialog box User groups the user belongs to.
|
Deactivate |
|
Description |
Descriptive text is available in the development system only and is not downloaded to the controller. |
Upload User from Device |
The data of the user management is uploaded from the controller. If user data is already configured. then it is overwritten. |
Download User to Device |
The data of the user management is downloaded to the controller. The existing user management on the controller is overwritten. |
Export User Management |
The drop-down list opens.
A standard dialog opens for saving the user management as a CSV file with any name in any directory. |
Import User Management |
A standard dialog opens for selecting the user management (in CSV format) from the file system. |
Settings for Download of User Data |
|
Download at each login |
The data of the user management is downloaded to the controller at login. Existing data is overwritten. |
No download at login |
The data of the user management is never downloaded to the controller, even if it changes. |
Allow decision on every download |
A Warning dialog box opens for you to accept or refuse the download. |
Access Rights for Elements |
|
Use group hierarchy |
The group in the first line of the Group list is the highest in the hierarchy. A group of a higher hierarchy cannot have fewer permissions for an element than a group of a lower hierarchy. |
Logout Behavior |
|
Change to start visualization at logout |
|
Login Settings |
|
Apply login restrictions |
|
Maximum number of authentication attempts |
Possible values: [1...10] When the maximum number of authentication attempts is reached, the user is locked out either temporarily or permanently, depending on the User lockout settings. |
User lockout |
|
The data for user management is saved to a CSV file in the following format:
User groups: ID;group name; automatic logoff TRUE/FALSE;logoff time;unit logoff time;permission to change user date TRUE/FALSE
Users: login name;full name;password encrypt TRUE/FALSE;password;group ID;user deactivated TRUE/FALSE
Use this format when you want to edit data for user management by means of any tool. If you set password encrypt
to FALSE
, then an unencrypted password can be used. In the example, the unencrypted password Yellow
was specified for the user Hugo
. If you import the CSV file with the command Import user management, then the password is encrypted automatically.
V1.0.0.1
User groups:
1;Admin;TRUE;1;Minute;TRUE
3;Operator;FALSE;1;Minute;FALSE
7;Service;FALSE;1;Minute;FALSE
0;None;FALSE;1;Minute;FALSE
4;Early and late shift;FALSE;1;Minute;FALSE
2;Early shift;TRUE;1;Minute;FALSE
6;Late shift;FALSE;1;Minute;FALSE
User:
Service;Service;TRUE;C08298D42A35732CFFB7DF43771B7607;2;FALSE
Operator;Operator;TRUE;3D94AB9540B025B07773DE7037F19837;3;FALSE
John;Blue;TRUE;62ED5DE29E5DD4164A01F3AF1B81EFA0;4;FALSE
Paul;White;TRUE;01E2CBD4AE5442D9EACE33669549A3CC;2;FALSE
Hugo;Green;FALSE;Yellow;6;FALSE
See also