With this element, you can integrate a trace graph in the visualization that monitors and displays variable values permanently. You configure the displayed trace graph in the element properties. In addition, you can add control elements that control the trace functionality. This is done manually or by using the Insert Elements for Controlling Trace command.
Configurations for the 'Trace' visualization element can be taken from the 'Trace' object.
See also