The Mathematics library offers different mathematically functionalities for Robotics and other libraries.
Characteristics of the Library
The following table indicates the characteristics of the library:
Characteristic |
Value |
---|---|
Library title |
Mathematics |
Company |
Schneider Electric |
Category |
oUtil oApplication/Util |
Component |
Core Libraries |
Default namespace |
SE_MATH |
Language model attribute |
|
Forward compatible library |
Yes (FCL) |
NOTE: For this library, qualified-access-only is set. This means, that the POUs, data structures, enumerations, and constants have to be accessed using the namespace of the library. The default namespace of the library is SE_MATH.