In FBD, implicit feedbacks can be programmed. For this, the involved variables must be declared as feedback variables and the rules mentioned below have to be observed when programming implicit feedbacks. Implicit feedbacks can, for example, be used to realize a storing behavior of a safety logic (e.g., flip-flop or cycle counter). The storing behavior of the safety logic which results from programming an implicit feedback may lead to a complex timing of the entire application.
| WARNING | |
|---|---|
Rules for programming implicit feedbacks in FBD
Implicit feedbacks in FBD can only be realized using variables but not via connection lines. When using lines, this is considered as forbidden explicit feedback (see figure (2) below).
Each variable that causes the implicit feedback must be formally declared as feedback variable.
This is done by selecting the 'Feedback' flag in the 'Variable' dialog or in the variables worksheet.
When using a variable without set flag in an implicit feedback, a compiler error results.
Only local variables can be declared as feedback variable.
To ensure a well-defined timing, feedback variables must not be written and read within one network (as shown in figure (3) below). Instead, the feedback logic must be divided in two separate networks as shown in figure (1) below.
Example