SET_LSB

This standard bit manipulation function contained in the <BIT_UTIL> library writes the value applied at input LSB to the least significant Byte of the bit string applied at input DATA.

Parameter

Data type

Description

LSB

BYTE

Value to be written to the LSB of DATA

DATA

WORD

Input bit string to be modified

OUT

WORD

Output bit string with modified written LSB