IAlarmAdditionalLatchVariables2.SetLatchVariablesAddress (METH)

METHOD SetLatchVariablesAddress

Dinamically set the pointer to the latch variable to use Use to set in the alarm FB the address of the latch variables to use, in case of not set by code generation. For internal use

InOut:

Scope

Name

Type

Comment

Input

paLatchVariables

POINTER TO BYTE

The pointer to use. It’s a pointer to ValueTypeBundle

usiCountLatchVariables

USINT

The effective size of the array above.