TYPE BUS_INFO : STRUCT
This structure provides basic information on a fieldbus:
eType: Type of fieldbus. See BUS_TYPE.
idSystem: Unique system ID for the identification of the fieldbus.
Bus Type
Interpretation
CANbus
Network ID
Profibus DP
MasterID (see also Master-FB Property)
DeviceNet
Network ID
EtherCAT
low DWORD of the MAC address of the master
Sercos III
CAA.gc_idMAX_IDENT
Profinet IO
MasterID (see also Controller-FB Property)
Modbus TCP
CAA.gc_idMAX_IDENT
Modbus RTU
CAA.gc_idMAX_IDENT
EtherNet/IP
IP address
AS Interface
CAA.gc_idMAX_IDENT
Ethernet
IP address
Serial Line
number of COM port
idInstance: Instance number in I/O configuration (starting by 0).
Example
First CANbus has instance number 0, second CANbus instance number 1, …
Attributes: |
qualified_only |
||||||||||||
InOut: |
|