IDevice.GetSpecificDeviceErrorAsync (METH)

METHOD GetSpecificDeviceErrorAsync : PROC_STATE

Returns the fieldbus specific device error.

Info

This is an asynchronous method. For easier handling use function block GetSpecificDeviceError.

Info

The interpretation of pData is fieldbus dependent and will be specified by the associated fieldbus driver.

InOut:

Scope

Name

Type

Comment

Return

GetSpecificDeviceErrorAsync

PROC_STATE

Input

eCmd

PROC_CMD

pData

CAA.PVOID

Pointer to memory

szSize

CAA.SIZE

Size of memory in bytes where pData is pointing to

Output

szCount

CAA.SIZE

Number of Bytes written to pData

eError

ERROR

error code if method fails