FUNCTION_BLOCK DirCreate EXTENDS CBM.ETrig
This function block creates a sub-directory in the standard directory. If the sub-directory already exists, an error message is generated. There may be restrictions concerning the specification of the directory name, e.g. only capital letters allowed, for different targets. The function ”FILE.GetProperty” shows these restrictions.
InOut:
|
Scope
|
Name
|
Type
|
Comment
|
Inherited from
|
Input
|
xExecute
|
BOOL
|
Rising edge: Action starts
Falling edge: Resets outputs
If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.
|
ETrig
|
Output
|
xDone
|
BOOL
|
TRUE: Action successfully completed
|
ETrig
|
xBusy
|
BOOL
|
TRUE: Function block active
|
ETrig
|
xError
|
BOOL
|
TRUE: Error occurred, function block aborts action
FALSE: No error
|
ETrig
|
Input
|
sDirName
|
CAA.FILENAME
|
Name of the new directory, absolute or relative path specification
|
|
xParent
|
BOOL
|
Create missing subdirectories; TRUE: missing sub-directories will be created automatically, FALSE: missing sub- directories will cause an error message
|
|
Output
|
eError
|
ERROR
|
Local library error ID (5104 - FILE_NOT_EXIST: Directory does not exist; 5105 - FILE_EXIST: Directory already exists )
|
|
|